This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25856EVM: question about auto-reverse mode

Part Number: BQ25856EVM
Other Parts Discussed in Thread: BQSTUDIO

In my test, the EN_REV bit will not enabled when the adapter is connected to the system. However, if the BQ25856EVM is already at reverse-mode without any adapter, the reverse mode will not be disabled automatically when adapter is connected. Meanwhile, the charging is stopped.

Does the reverse mode still work when the reverse-mode is on and the adapter is connected? For example, if I set the reverse voltage to 12V, and the adapter voltage is 24V, will it be a problem when the adapter is connected to VAC and the reverse mode is on?

  • Hi,

    We have received your post and the investigation will take some time. Thank you for your patience.

  • Hi,

    The device cannot set EN_REV when there is a power good status. If you set the reverse voltage to 12V and EN_REV, the reverse voltage register will remain 12V until it is reset, but the device will not enter reverse mode.

  • Thank you for your reply!

    However, I'm sorry that I don't think this resolved my issue. May I explain my test with more detail?

    First, I activated the reverse mode and observed that the evaluation board’s VAC output was at 12V.
    Next, I powered on the connected 24V external adapter. At this point, the VAC voltage rose to 24V; however, monitoring through BQstudio showed that the reverse mode had not been disabled. 

    I understand that you mean the reverse mode is not actually activated at this time, but I would like to know if it is also normal for EN_REV to remain enabled under these conditions?

  • Hi,

    Yes, this would be normal. The device cannot automatically exit the reverse mode. It is recommended to set EN_REV=0 to exit reverse mode.