Part Number: BQ25856EVM
Other Parts Discussed in Thread: BQSTUDIO
In my test, the EN_REV bit will not enabled when the adapter is connected to the system. However, if the BQ25856EVM is already at reverse-mode without any adapter, the reverse mode will not be disabled automatically when adapter is connected. Meanwhile, the charging is stopped.
Does the reverse mode still work when the reverse-mode is on and the adapter is connected? For example, if I set the reverse voltage to 12V, and the adapter voltage is 24V, will it be a problem when the adapter is connected to VAC and the reverse mode is on?