This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPS61252的应用demo电路

Other Parts Discussed in Thread: TPS61252

TPS61252的技术手册中有下列描述:

11.2.2.1 Output Voltage Setting
The output voltage is calculated by Equation 5:
(5)
To minimize the current through the feedback divider network, R2 should be between 180 kΩ and 360 kΩ. The
sum of R1 and R2 should not exceed ~1 MΩ, to keep the network robust against noise. For the example, R1 is
768 kΩ and R2 is 243 kΩ.

R1+R2<1M 但是demo电路取的768和243,两者的和超过了1M啊,该以哪个为准?

  • 对于TPS61252,R2不在小信号环路内,我们写普通运放结构的误差放大器和补偿网络的传递函数时,可以看到只有R1才会与零极点位置有关,R2是不出现在这个传递函数内的,它主要的作用是作为直流偏置电阻(有时会影响运放的带宽),对于其阻值不能太大导致偏置电流不够,也不能太小导致偏置的功耗过大。

    对于给定了R2的范围,两者的和在1M欧姆以下或1M欧姆左右都可以,不要超过1M欧姆太多即可(这个要求实际是指R1不要选太大影响噪音信号的传递)

    实际选择中选择低温漂 高精度的电阻类型。

  • 楼主如果在以后的工作中遇到采用跨导型结构的误差放大器,而不是最常见的普通运放架构的误差放大器,此时则需要留意此时R2会影响到跨导型误差放大器输入级的极点位置。

    谢谢!