This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63020: TPS63020

Part Number: TPS63020

使用该DC-DC设计一个升降压电路,参考规格书里给出的典型应用电路,元器件参数也按照要求设计。

1、设计指标:

      输入:2.5V---5.5V

      输出:3.8V/1.2A

 2、测试结果:

      当输入电压<4.2V时,基本满足设计指标;

      当输入电压为4.2V---5.5V时,输出电压为1V左右,电流为0.25A左右。

      

      请问是什么原因?怎样改进?