Other Parts Discussed in Thread: UCC3895, UCC28950
最近调试UCC2890时发现A,B驱动波形正常,而C,D驱动会出现大小波,主要表现在BOOST模式情况下,具体表现为boost时,D管的驱动宽度有时很窄,有时正常,这样导致C管有时会比较比较宽的驱动,请问这是芯片固有的特性吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,应该是环路问题,或者COMP pin 被干扰了,左右抖动就是说明相移角在不断变化,或者谢谢。
Land wind:
首先,谢谢回复!
我尝试用外部运放做环路,把EA-和comp直接在芯片上相连(PCB上原来EA-和comp脚走线直接割断),外部运放输出直接到EA+,还是没有一点变化,
但我今天做了一个有趣的尝试,用UCC3895做了一块小板,替换UCC28950,原来采样和控制环路,工作很好,不再抖动了。
thanks!
你好,
如果是很小的抖动,只是小于200ns以内的话,是正常的,原因是变压器变比和电流模式造成的,具体你可以参考附件中的page19的介绍,谢谢。

Land wind,你好:
按你这样说就很好解释了,我就可以理解了,我之前对UCC3895比较熟悉,所以判断这种抖动是有问题的;
对于用UCC3895不会抖动,我想是不是:我这边原理图上对UCC3895的7脚Ct信号通过一个电阻到3脚RAMP,一种斜坡补偿,