Part Number: BQ4050
Hi TI Experts
We have designed a 3S3P NMC battery power management solution using the BQ4050. After re-reading the battery log records following a period of usage, as shown in the table below, we observed the following:
While most battery cycle counts range between 100–200 cycles, the MaxError values are highly scattered. At 200 cycles, for instance, MaxError values include 2%, 49%, and even 100%. However, the SOH and FCC of the batteries show no significant abnormalities. Could you please help clarify the following questions:
1. What is the calculation method for MaxError? There is no relevant explanation in the TRM.
2. What causes such a wide dispersion in MaxError values? Is this phenomenon normal?
3. Can such scattered MaxError values indicate a mismatch between BQ4050 parameters and the battery cells? Could it be due to issues in BQ4050 parameter design, or improper settings during battery usage?
4. Under normal circumstances, what is the approximate relationship between MaxError and cycle count? Is there a rough estimation method?
5. How reliable is MaxError? Can it be used as a criterion for determining battery degradation?
6. If the answer to question 5 is affirmative, what is the method for judging battery degradation using MaxError? If not, aside from SOH, could you provide examples of other parameters in the BQ4050 log that can be used to assess battery degradation?
BQ4050 log.xlsxThe complete gg file and log file are attached. Please review and confirm as soon as possible. Thank you!
| MaxErr | RSOC | ASOC | SOH | RemCap | FullChgCap | ChgCurr | ChgVolt | BattStat | CycleCnt |
| 34 | 58 | 59 | 100 | 5297 | 9213 | 3750 | 12600 | 0x00C0 | 219 |
| 14 | 70 | 71 | 100 | 6344 | 9186 | 3750 | 12600 | 0x00C0 | 225 |
| 26 | 70 | 72 | 100 | 6433 | 9195 | 3750 | 12600 | 0x00C0 | 216 |
| 46 | 100 | 102 | 100 | 9142 | 9188 | 44 | 12600 | 0x00E0 | 214 |
| 13 | 94 | 96 | 100 | 8556 | 9190 | 3750 | 12600 | 0x00C0 | 200 |
| 100 | 52 | 53 | 100 | 4766 | 9263 | 3750 | 12600 | 0x00C0 | 210 |
| 8 | 86 | 87 | 100 | 7753 | 9095 | 3750 | 12600 | 0x00C0 | 226 |
| 2 | 67 | 67 | 99 | 5970 | 8951 | 3750 | 12600 | 0x00C0 | 224 |
| 2 | 77 | 77 | 100 | 6901 | 9051 | 3750 | 12600 | 0x00C0 | 167 |
| 8 | 96 | 97 | 100 | 8727 | 9146 | 44 | 12600 | 0x00E0 | 214 |
| 8 | 99 | 101 | 100 | 9028 | 9163 | 44 | 12600 | 0x00E0 | 208 |
| 4 | 100 | 99 | 99 | 8836 | 8870 | 44 | 12600 | 0x00E0 | 203 |
| 100 | 88 | 90 | 100 | 8063 | 9263 | 3750 | 12600 | 0x00C0 | 212 |
| 3 | 87 | 87 | 100 | 7757 | 8962 | 3750 | 12600 | 0x00C0 | 212 |
| 16 | 87 | 90 | 100 | 8077 | 9305 | 3750 | 12600 | 0x00C0 | 214 |
| 15 | 91 | 93 | 100 | 8293 | 9200 | 3750 | 12600 | 0x00C0 | 216 |
| 100 | 67 | 69 | 100 | 6136 | 9263 | 3750 | 12600 | 0x00C0 | 210 |
| 33 | 65 | 67 | 100 | 6019 | 9373 | 3750 | 12600 | 0x00C0 | 212 |
| 39 | 65 | 66 | 100 | 5871 | 9060 | 3750 | 12600 | 0x00C0 | 220 |
| 49 | 94 | 99 | 100 | 8844 | 9466 | 3750 | 12600 | 0x00C0 | 192 |
| 48 | 99 | 100 | 100 | 8976 | 9107 | 44 | 12600 | 0x00E0 | 199 |
| 37 | 78 | 80 | 100 | 7145 | 9241 | 3750 | 12600 | 0x00C0 | 218 |
| 100 | 87 | 90 | 100 | 8031 | 9263 | 3750 | 12600 | 0x00C0 | 159 |
| 100 | 100 | 103 | 100 | 9204 | 9263 | 44 | 12600 | 0x00E0 | 163 |
| 26 | 92 | 96 | 100 | 8621 | 9416 | 3750 | 12600 | 0x00C0 | 125 |
| 100 | 100 | 103 | 100 | 9200 | 9263 | 44 | 12600 | 0x00E0 | 103 |
| 100 | 65 | 67 | 100 | 5962 | 9263 | 3750 | 12600 | 0x00C0 | 128 |
| 27 | 69 | 71 | 100 | 6323 | 9269 | 3750 | 12600 | 0x00C0 | 134 |
| 5 | 100 | 100 | 100 | 8976 | 9040 | 44 | 12600 | 0x00E0 | 128 |
| 100 | 67 | 69 | 100 | 6125 | 9263 | 3750 | 12600 | 0x00C0 | 134 |
| 2 | 63 | 63 | 100 | 5621 | 9004 | 3750 | 12600 | 0x00C0 | 133 |
| 2 | 77 | 78 | 100 | 6970 | 9149 | 3750 | 12600 | 0x00C0 | 132 |
| 11 | 53 | 55 | 100 | 4948 | 9349 | 3750 | 12600 | 0x00C0 | 121 |
| 100 | 99 | 102 | 100 | 9170 | 9263 | 3750 | 12600 | 0x00C0 | 131 |
| 100 | 77 | 79 | 100 | 7068 | 9263 | 3750 | 12600 | 0x00C0 | 133 |
| 100 | 76 | 79 | 100 | 7032 | 9263 | 3750 | 12600 | 0x00C0 | 105 |
| 100 | 87 | 90 | 100 | 8042 | 9263 | 3750 | 12600 | 0x00C0 | 57 |
| 2 | 100 | 101 | 100 | 9052 | 9097 | 44 | 12600 | 0x00E0 | 128 |
| 100 | 65 | 67 | 100 | 5946 | 9263 | 3750 | 12600 | 0x00C0 | 135 |
| 100 | 65 | 67 | 100 | 5946 | 9263 | 3750 | 12600 | 0x00C0 | 135 |
| 32 | 86 | 87 | 100 | 7744 | 9075 | 3750 | 12600 | 0x00C0 | 132 |
| 100 | 86 | 89 | 100 | 7957 | 9263 | 3750 | 12600 | 0x00C0 | 130 |
| 100 | 100 | 103 | 100 | 9217 | 9263 | 44 | 12600 | 0x00E0 | 134 |
| 100 | 95 | 97 | 100 | 8708 | 9263 | 3750 | 12600 | 0x00C0 | 141 |
| 100 | 73 | 75 | 100 | 6692 | 9263 | 3750 | 12600 | 0x00C0 | 131 |
| 100 | 92 | 95 | 100 | 8481 | 9263 | 3750 | 12600 | 0x00C0 | 136 |
| 16 | 62 | 63 | 100 | 5651 | 9193 | 3750 | 12600 | 0x00C0 | 127 |
| 30 | 87 | 89 | 100 | 7966 | 9205 | 3750 | 12600 | 0x00C0 | 138 |
| 4 | 65 | 67 | 100 | 5957 | 9226 | 3750 | 12600 | 0x00C0 | 134 |
| 25 | 70 | 72 | 100 | 6428 | 9292 | 3750 | 12600 | 0x00C0 | 126 |
| 27 | 55 | 57 | 100 | 5042 | 9284 | 3750 | 12600 | 0x00C0 | 133 |
| 17 | 94 | 97 | 100 | 8676 | 9311 | 3750 | 12600 | 0x00C0 | 126 |
| 8 | 74 | 77 | 100 | 6884 | 9371 | 3750 | 12600 | 0x00C0 | 132 |
| 100 | 64 | 65 | 100 | 5844 | 9263 | 3750 | 12600 | 0x00C0 | 119 |
| 4 | 78 | 80 | 100 | 7166 | 9292 | 3750 | 12600 | 0x00C0 | 134 |
| 31 | 92 | 97 | 100 | 8723 | 9490 | 3750 | 12600 | 0x00C0 | 128 |
| 100 | 79 | 81 | 100 | 7245 | 9263 | 3750 | 12600 | 0x00C0 | 130 |
| 6 | 88 | 91 | 100 | 8119 | 9321 | 3750 | 12600 | 0x00C0 | 122 |
| 27 | 67 | 67 | 100 | 5967 | 9016 | 3750 | 12600 | 0x00C0 | 122 |
| 5 | 94 | 97 | 100 | 8642 | 9221 | 3750 | 12600 | 0x00C0 | 110 |
| 8 | 96 | 100 | 100 | 8966 | 9369 | 3750 | 12600 | 0x00C0 | 126 |
| 7 | 96 | 98 | 100 | 8798 | 9243 | 3750 | 12600 | 0x00C0 | 130 |
| 100 | 22 | 23 | 100 | 2007 | 9263 | 3750 | 12600 | 0x00C0 | 131 |
| 33 | 78 | 81 | 100 | 7238 | 9299 | 3750 | 12600 | 0x00C0 | 130 |
| 15 | 94 | 95 | 100 | 8461 | 9084 | 3750 | 12600 | 0x00C0 | 86 |
| 27 | 50 | 51 | 100 | 4562 | 9188 | 3750 | 12600 | 0x00C0 | 136 |
| 100 | 87 | 90 | 100 | 8042 | 9263 | 3750 | 12600 | 0x00C0 | 127 |
| 31 | 78 | 82 | 100 | 7368 | 9505 | 3750 | 12600 | 0x00C0 | 131 |
| 19 | 100 | 102 | 100 | 9119 | 9165 | 44 | 12600 | 0x00E0 | 137 |
| 100 | 61 | 63 | 100 | 5605 | 9263 | 3750 | 12600 | 0x00C0 | 133 |
| 6 | 68 | 69 | 100 | 6192 | 9184 | 3750 | 12600 | 0x00C0 | 132 |
| 5 | 72 | 75 | 100 | 6716 | 9432 | 3750 | 12600 | 0x00C0 | 132 |
| 17 | 55 | 57 | 100 | 5051 | 9214 | 3750 | 12600 | 0x00C0 | 132 |
| 34 | 95 | 97 | 100 | 8695 | 9158 | 3750 | 12600 | 0x00C0 | 134 |
| 14 | 74 | 76 | 100 | 6810 | 9299 | 3750 | 12600 | 0x00C0 | 127 |
| 100 | 94 | 96 | 100 | 8621 | 9263 | 3750 | 12600 | 0x00C0 | 107 |
| 100 | 69 | 71 | 100 | 6338 | 9263 | 3750 | 12600 | 0x00C0 | 133 |
| 100 | 95 | 98 | 100 | 8737 | 9263 | 3750 | 12600 | 0x00C0 | 126 |
| 5 | 98 | 99 | 100 | 8857 | 9058 | 44 | 12600 | 0x00E0 | 218 |
| 8 | 99 | 101 | 100 | 9012 | 9130 | 44 | 12600 | 0x00E0 | 215 |
| 38 | 100 | 103 | 100 | 9226 | 9234 | 44 | 12600 | 0x00E0 | 224 |
| 2 | 99 | 100 | 100 | 8995 | 9092 | 44 | 12600 | 0x00E0 | 134 |
| 2 | 50 | 50 | 100 | 4466 | 9033 | 3750 | 12600 | 0x00C0 | 163 |
| 2 | 50 | 51 | 100 | 4536 | 9244 | 3750 | 12600 | 0x00C0 | 192 |
| 4 | 99 | 102 | 100 | 9105 | 9205 | 44 | 12600 | 0x00E0 | 206 |
| 11 | 99 | 101 | 100 | 9053 | 9168 | 44 | 12600 | 0x00E0 | 208 |
| 2 | 51 | 50 | 99 | 4497 | 8914 | 3750 | 12600 | 0x00C0 | 210 |
| 20 | 11 | 11 | 100 | 984 | 9120 | 3750 | 12600 | 0x00C0 | 149 |
| 16 | 99 | 100 | 100 | 8979 | 9148 | 44 | 12600 | 0x00E0 | 207 |
| 2 | 57 | 59 | 100 | 5284 | 9315 | 3750 | 12600 | 0x00C0 | 9 |
| 4 | 100 | 100 | 100 | 8931 | 9016 | 44 | 12600 | 0x00E0 | 141 |
| 16 | 100 | 103 | 100 | 9205 | 9210 | 44 | 12600 | 0x00E0 | 133 |
| 2 | 31 | 33 | 100 | 2962 | 9622 | 3750 | 12600 | 0x00C0 | 2 |
| 38 | 98 | 100 | 100 | 8934 | 9138 | 44 | 12600 | 0x00E0 | 182 |
| 100 | 29 | 30 | 100 | 2651 | 9364 | 3750 | 12600 | 0x00C0 | 3 |
| 2 | 50 | 51 | 100 | 4581 | 9280 | 3750 | 12600 | 0x00C0 | 49 |
| 100 | 100 | 103 | 100 | 9231 | 9263 | 44 | 12600 | 0x00E0 | 118 |
| 2 | 12 | 12 | 100 | 1068 | 9699 | 3750 | 12600 | 0x00C0 | 8 |
| 100 | 100 | 103 | 100 | 9257 | 9263 | 44 | 12600 | 0x00E0 | 125 |
| 17 | 99 | 102 | 100 | 9153 | 9267 | 44 | 12600 | 0x00E0 | 133 |
| 2 | 99 | 102 | 100 | 9163 | 9260 | 44 | 12600 | 0x00E0 | 133 |
| 2 | 74 | 76 | 100 | 6759 | 9225 | 3750 | 12600 | 0x00C0 | 48 |
| 8 | 100 | 103 | 100 | 9222 | 9253 | 44 | 12600 | 0x00E0 | 128 |
| 14 | 99 | 104 | 100 | 9286 | 9404 | 44 | 12600 | 0x00E0 | 130 |
| 100 | 100 | 103 | 100 | 9258 | 9263 | 44 | 12600 | 0x00E0 | 129 |
| 10 | 100 | 103 | 100 | 9208 | 9214 | 44 | 12600 | 0x00E0 | 133 |
| 2 | 99 | 101 | 100 | 9084 | 9182 | 44 | 12600 | 0x00E0 | 134 |
| 2 | 33 | 33 | 100 | 2948 | 9177 | 3750 | 12600 | 0x00C0 | 109 |
| 100 | 99 | 102 | 100 | 9170 | 9263 | 3750 | 12600 | 0x00C0 | 125 |
| 8 | 98 | 101 | 100 | 9024 | 9235 | 44 | 12600 | 0x00E0 | 103 |
| 2 | 50 | 50 | 100 | 4488 | 9048 | 3750 | 12600 | 0x00C0 | 123 |
| 100 | 100 | 103 | 100 | 9257 | 9263 | 44 | 12600 | 0x00E0 | 132 |
| 10 | 31 | 33 | 100 | 2883 | 9300 | 3750 | 12600 | 0x00C0 | 79 |
| 6 | 100 | 102 | 100 | 9141 | 9184 | 44 | 12600 | 0x00E0 | 132 |
| 2 | 1 | 1 | 100 | 24 | 9203 | 3750 | 12600 | 0x02D0 | 128 |
| 25 | 30 | 33 | 100 | 2919 | 9775 | 3750 | 12600 | 0x00C0 |
83 |