This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-R2: Cannot Locate Registers for "Fast Resistance Scaling" Feature Described in TRM

Part Number: BQ34Z100-R2

Dear TI Support Team,

I am working with the BQ34Z100-R2 fuel gauge and have been studying the Technical Reference Manual (SLUUC05A, Revised August 2023) to implement the "Fast Resistance Scaling" feature described in Section 3.11.

The feature is explained in detail, and I understand its purpose to improve RSOC convergence at low temperatures and high discharge rates. However, I am unable to locate the critical registers needed to control and monitor this function within the Data Flash Summary (Table 7-1).

Specifically, I cannot find the following two items mentioned in the TRM:

  1. The Enable Bit (RSOC_CONV or similar):

    • Section 3.11.1 states: *"When enabled with IT Gauging Configuration[RSOC_CONV] = 1, fast resistance scaling becomes active..."*

    • I have thoroughly searched Table 7-1 and the Gas Gauging -> IT Cfg subclass but cannot find a register or bit named RSOC_CONV or any obvious enable control for this feature.

  2. The Status Register (Cell 1 RaScale):

    • Section 3.11.1 and 3.11.2 refer to the Cell 1 RaScale register, which holds the calculated resistance scale factor.

    • This register is also absent from Table 7-1.

The dependent configuration parameters for this feature (Term Voltage DeltaFast Scale Start SOC, etc.) are present in the table and accessible. However, without the ability to enable the feature or read its status, I cannot verify its operation or integrate it into our system.

My questions are:

  1. What is the exact data flash location (Subclass ID and Offset) or command for the Fast Resistance Scaling enable control (RSOC_CONV)?

  2. What is the exact data flash location or command to read the Cell 1 RaScale status value?

  3. Is it possible that this feature is controlled by a bit within an existing multi-bit configuration register that is not explicitly named in the summary table? If so, which register and which bit?

  4. Could this be a discrepancy between the TRM documentation and the current firmware version?

Any guidance or clarification you can provide would be immensely helpful. Thank you for your time and support.

Best regards,

  • 您好,
    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • Hello ,

    What is the exact data flash location (Subclass ID and Offset) or command for the Fast Resistance Scaling enable control (RSOC_CONV)?

    这个有错误,对应功能位于pack configuration B 的 FConvEn.

    • What is the exact data flash location or command to read the Cell 1 RaScale status value?

    • Is it possible that this feature is controlled by a bit within an existing multi-bit configuration register that is not explicitly named in the summary table? If so, which register and which bit?

    • Could this be a discrepancy between the TRM documentation and the current firmware version?

    这是文档错误,并且在此芯片上没有报告此问题。