UCC28782: UCC28782反激变换器开关频率设置,FB电压反馈以及辅助升压变换器的一些问题

Part Number: UCC28782
Other Parts Discussed in Thread: , PMP10726, PMP22322

尊敬的工程师:
您好!我是电力电子领域的初学者,在尝试使用 UCC28782 设计反激式电源时遇到了一些问题,希望能得到您的帮助:
  1. 该芯片的开关频率是如何确定的?我在数据手册中看到了关于 fBUR 突发频率的描述,但没有找到关于数据包内单个开关周期的相关信息。请问能否解释一下在 AAM(自动调节模式)下的开关频率以及数据包内单个开关频率是如何确定的?我注意到文档中提到其开关频率为最高 1.5MHz 的可变频率,但似乎没有用于频率设置的引脚或其他元件。还是说我无需考虑这个问题,芯片会自适应设置合适的频率?
  2. 在参考设计中,我注意到 FB 引脚似乎通过快充芯片的内部 DAC 进行反馈。它是否通过 DAC 输出的不同偏置电压来设置 PD 芯片的不同输出电压?设置不同电压的常规方案是什么?选择 4 个分压电阻网络进行切换是个好主意吗?
  3. 对于辅助绕组引出的 BIN、BSW、BGND 所组成的升压转换器的功能,我存在一些疑问。我的理解是它用于为 VDD 供电,整体最大功率为 18.5V、0.33A。是不是因为功率较大且电压特殊,所以才单独设置了一个升压转换器?
希望能得到您的帮助,非常感谢!

Dear Engineer,
Hello, I am a beginner in power electronics. I encountered some problems while trying to design a flyback power supply using UCC28782 and hope to get your help:
1.How is the switching frequency of the chip determined? I saw the description of fBUR burst frequency in the datasheet, but I couldn't find relevant information about the individual switching cycles within the data packet. Could you please explain how the switching frequency in AAM (Auto Adjustment Mode) and the individual switching frequency within the data packet are determined? I noticed that the document mentions its switching frequency is a variable frequency with a maximum of 1.5 MHz. However, there seems to be no pin or other component for frequency setting. Could you please tell me how to set the switching frequency? Or I dont need to consider about it ,the chip will adapt by itself?
2.In the reference design, I noticed that the FB pin seems to use feedback through the internal DAC of the fast-charging chip. Does it set different output voltages of the PD chip through different bias voltages output by the DAC? What is the conventional scheme for setting different voltages? Is choosing 4 voltage divider resistor networks for switching a good idea?
3.I have some questions about the function of the boost converter composed of BIN, BSW, and BGND from the auxiliary winding. My understanding is that it is used to supply power to VDD, with an overall maximum power of 18.5V and 0.33A. Is a separate boost converter used because the power is relatively large and the voltage is special?
I hope to receive your help. Thank you very much!

  • 您好,收到了您的案例,调查需要些时间,感您的耐心等待。

  • 您好

    开关频率将由芯片根据负载情况自动决定。

    我无法理解第二个问题,你能提供参考设计链接吗?

    升压转换器用于具有宽输出电压范围的应用,以将VDD保持在推荐的工作范围内。

  • 非常感谢您的回复,我明白了第一个和第三个问题

    对于第二个问题,例如PMP10726,将输出反馈通过一个恒定的LDO进行分压来控制输出电压。以及类似PMP22322,在一个板子上设置多个电阻分压通道,通过数字控制来选择合适的通路。请问这样合适吗?或者类似UCC28782EVM-030,我发现其FB通过PD芯片WT6630P的CATH引脚进行输出反馈,PD芯片内部有一个8051,我觉得这个引脚可能是一个DAC,方案将DAC的输出电压作为分压源,从而控制输出电压?

  • 您好

    据我了解,问题是如何在需要宽输出电压的应用中为每个输出电压设置参考电压,否则请纠正我。

    因此,考虑到上述情况,通常有两种方式:

    1) 使用单一参考电压,手动或通过跳线改变输出电压分压器中的较低电阻值。

    2) 在适配器、USB PD控制器(例如WT6636F)等应用中,通过改变PD控制器内的参考电流来设置参考电压。

  • 好的 我想我明白了 感谢您的解答!