This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25830A-Q1: Communication pulse problem after power short circuit

Part Number: TPS25830A-Q1

When short circuiting USB-OTG-POWER to GND (using a wire directly connected to GNG),

DP_OUT、DM_OUT will experience abnormal downward movement,the value is approximately -660mV to -800mV.

At this point, the communication between the rear stage and 25830 has exceeded the absolute maximum ratings of the HUB IC(-0.5V).

What is the reason for this abnormal pulse? How can it be eliminated?