Other Parts Discussed in Thread: TPS5430, BQ24295, BQ24195, BQ24035, BQ24296
请问如下需求如何实现:
电源1:备份电池是3.7V聚合锂电池,
电源2:TPS5430从12V转成的4V
用电设备的电压范围:3.4-4.5V
要求:当电源2有上电时从电源2取电,同时对电源1进行充电,当电源2断开时,从电源1取电,切换过程用电设备不能断电
麻烦指导,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 你的聚合物锂电池是不能直接用电压源充电的,需要一个专门的锂电池充电芯片来完成。否则有严重的安全问题。
2. 建议用一个TPS5430将电压降到5V,然后接一个BQ24296带路径管理,即BQ24296可以同时给电池和系统供电,当TPS5430断电后,系统供电自动由电池获取
完美!