1、用评估板BQ27531EVM+EV2400+BQEVSW上位机软件最后生成的dffs文件,这个dffs文件里面是一些I2C命令和数据吗?可以通过什么工具直接看到里面的内容吗 ?生成该dffs文件后,评估板BQ27531EVM里的电量管理芯片BQ27531已经下载好了程序了吧?然后CPU怎么用这个dffs文件对板载上的BQ27531、BQ24195进行编程控制下载相关参数?
2、打开BQEVSW这个上位机软件时弹出显示EV2300没有连接,可以用EV2400连接该上位机软件使用吗?或者还是说EV2300和EV2400这两个不同的下载器对应不同的上位机软件?如果是这样的话,那EV2400对应的上位机软件是什么?
3、在烧写电芯参数步骤3 CHEM-ID时,需要将log的数据保存下来用MATHCAD程序计算CHEM_ID,请问有MATCHCAD这个软件的连接吗?