This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22811: TPS22811LRPWR Schematic review

Part Number: TPS22811

Hi Team,

Please help review the SCH design for the TPS22811 with design specifications: Vin= 12V0, Iout= 2A.

EN is controlled by MCU, if voltage is UVLO, the external discharge circuit will work.

image.png

  • Hello, we have received your case and the investigation will take some time. Thank you for your patience.

  • Hello, I was wondering if there is any update about this question?

  • 1. Transient protection is missing. We recommend using TVS diode at the input and Schottky diode at the output to help against transients which are generated in events like hot-plug or short circuit and can cross the absolute maximum of the device resulting in permanent damage to device.

    2. Can you check the EN pin connection , if you want to use it , you need to connect the resistor ladder from VIN pin to gnd.

    3. The PG pin is recommended to pull up with resistor of value 47K ohm

    4. Connecting the IMON pin to ground disables the active current limit protection during startup