寻求外围电路类似于TL494形式的脉宽调制器,工作温度为-40-125度的,之前想用TL494芯片,但是发现TL494的温度只能达到85度,需要寻找一片工作温度更高的脉宽调制芯片
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
你是什么应用,做什么电路,是不是可以考虑用converter,集成mosfet更简单,谢谢。
我主要的应用是将200V-600V的高压直流,使用TL494与自举芯片IR2110的配合驱动高压MOSFET管7N90,将高压直流转化成直流24V输出