This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电池容量配置问题

Design Capacity: 和Design Energy: 是指一个电池的容量还是电池包的呢,我用的是电池包,4个电池并联后再两组串联,7.2v  15A的磷酸铁锂电池,这两个参数应该怎么配置呢?Number of Series Cells应该填8还是2呢

  • design capacity  = 并联数 * 单体电池容量

    design energy  = design capacity * 单体电池电压* 串联个数

    number of series cells = 单体电池串联个数

    注意这个单体电池的概念。实际上你所认为的7.2V铁锂电池,内部应该是两个电芯串联组成。有些厂家组包的时候,两个串联组成一个包。

    但是对电量计来说,都是正对单节电芯来说的。