在手册中IADJ脚没有使用并用一个10M欧和0.01UF电容串联在此,
1、如果我要使用IADJ那我最终实现的是限制最大电流输出还是动态模拟调光功能?
2、如果我想实现动态可调,是否可以像图二般通过一个电阻和电位器分压构成的0.18V-1.8V对IADJ进行模拟调光10:1?此时需要保留手册中的10M欧和0.01UF电容吗?
我的问题很紧急,麻烦TI的工程师尽快回复我
您好,
已经收到了您的案例,调查需要些时间,感谢您的耐心等待
Links ,Please reply to me as soon as possible. My project schedule is very tight.