This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14006高低温后出现啸叫

Other Parts Discussed in Thread: LMR14006

 我们用LMR14006YDDC给MCU供电,在做完高低温(85℃和-40℃)试验后,常温上电有轻微啸叫声。定位后发现是LMR14006YDDC电源电路部分

电感L24啸叫。测试电源输出纹波,见图1;

由图001可以看出,有一个大概12K左右的锯齿波纹波,幅度约40MV,导致电感L24发声。

图2是正常电源LMR14006YDDC的纹波图,由图可看出也有一个大概20mv 20KHz的锯齿波。

我们设计电源开关频率为2.1MHz,麻烦帮忙分析下这个12K(20K)左右锯齿波是怎么产生的,有消除的办法吗?谢谢!

电源部分设计如下: