This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25619E: How to enable BATFET fully system reset

Part Number: BQ25619E

1) In the datasheet, these informations are mentioned.

" When BATFET_RST_EN = 1 and BATFET_DIS = 0, BATFET full system reset function is enabled"

"Enable BATFET reset function when REG07[5] is also 1. (default)"  REG07[5] is BATFET_DIS bit.

I think there is a contradiction between these two descriptions.

I guess that "BATFET_RST_EN = 1 and BATFET_DIS = 0" will enanle full system reset function, then set "BATFET_DIS = 1" to full system reset. Please help confirm.

 

2)if want to enter ship mode, then we should set "BATFET_RST_EN = 0 and BATFET_DIS = 1". Please help confirm.