LM2596 用稳压电源输入电压9V,输入电流260mA左右,负载为5V输出,LED灯驱动电流400mA左右,只要一开LED灯,无线通讯就不稳定,会断信号通讯不了,此时纹波100mV左右,噪声300mV左右,关掉LED,无线通讯链接正常,此时纹波在50mV以下,噪声在150mV以下;调试时在输入9V上加680UF电解电容或输出5V上加220UF,也没有改善,基本没有变化,


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM2596 用稳压电源输入电压9V,输入电流260mA左右,负载为5V输出,LED灯驱动电流400mA左右,只要一开LED灯,无线通讯就不稳定,会断信号通讯不了,此时纹波100mV左右,噪声300mV左右,关掉LED,无线通讯链接正常,此时纹波在50mV以下,噪声在150mV以下;调试时在输入9V上加680UF电解电容或输出5V上加220UF,也没有改善,基本没有变化,


说实话,你的问题描述很多文字,但我们还是不了解你的系统,LED接在哪儿,通讯模块跟LM2596的关系(是2596的负载?)等等。。。你发一个完整的系统电流图出来会比较好,