This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: BQ4050如何通过I2C指令设置Enabled Protections D的UTD?

Part Number: BQ4050
Other Parts Discussed in Thread: BQSTUDIO

我监控了EV2300发出来的设置Enabled Protections D的UTD,具体数据如下:       

       0x16 0x44 0x22

       0x80 0x44 0x0F

       0xBE 0xOA 0x02 0x0E 0x06 0x66 0x08 0x33

       0x04 0x33 0x04 0x33 0x04 0x00 0x28 0x03

       0xA8 0x03 0xA8 0x03 0xA8 0x03 0x97 0x04

       0x00 0x8B 0x06 0x00 0xB2 0x00 0x00 0x86

      

       0x16,0x44 0x22

       0x80 0x44 0x0F

       0xBF 0x06 0x00 0x41 0x80 0x8C 0x81 0x0E

       0xC0 0x81 0x30 0x20 0xCC 0x10 0x01 0x50

       0x07 0x50 0x03 0xD4 0x01 0xDA 0x00 0xF2

       0xE0 0x24 0x06 0x58 0x34 0x02 0x90 0x00

       0x01 0x0D

      

       0x16 0x44 0x22

       0x80 0x44 0x03

       0x5F 0x02 0x00 0x07 0x80 0xC6 0xE0 0x83

       0x60 0x81 0x18 0x20 0x98 0x20 0x04 0x40

       0x0F 0xA0 0x0F 0xA0 0x07 0x50 0x07 0x2E

       0x0C 0x00 0x8B 0x06 0x00 0xB2 0x00 0x00

       0x85

      

       0x16,0x44 0x22

       0x80 0x44 0x07

       0x5F 0x02 0x00 0x83 0x01 0x8C 0xC0 0x83

       0x60 0x83 0x60 0x41 0x38 0x20 0x02 0xA0

       0x07 0x50 0x07 0xA4 0x01 0xD4 0x01 0xCB

       0x02 0x80 0x63 0xE0 0x68 0x02 0x90 0x00

       0x06 0x1A

     

       0x16,0x44 0x22

       0x80 0x44 0x07

       0xBE 0x0A 0x01 0x0E 0x06 0x31 0x02 0x19

       0x02 0x18 0x81 0x0C 0x81 0x00 0x62 0x80

       0x3D 0x80 0x3D 0x80 0x1E 0x40 0x1E 0xB8

       0x32 0x01 0x0D 0x01 0x40 0x2C 0x00 0x00

       0x18

 

请问,这些数据怎么解析?我应该发送什么指令,才可以设置Enabled Protections D的UTD?