This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5069: LM5069驱动多对并联MOS时对Qg有无特殊要求

Part Number: LM5069

请问:比如驱动3对背靠背MOS管,每对MOS管流过20A电流;所有MOS管的Qg总和或者Ciss有无最大值要求?

看论坛其它问答,说是可以驱动6个MOS管。

我的实验电路就是使用一片LM5069驱动多路并联的背靠背mos,给电阻负载供电:输入50v,电阻15欧,输出无电容。

我实验时发现驱动1路下面参数的MOS管,空载基本能打开mos开关,栅极电压比VIN高约10v;但是带15欧负载,输入上电时经常不能打开MOS开关。

栅极电荷量(Qg) 63nC@10V
输入电容(Ciss) 4.406nF@50V

如果是下面参数的mos管1对背靠背,空载时大功率可以打开mos;如果是3对背靠背,空载时打不开MOS,此时栅极输出电压等于VIN, 如果接上负载,栅极输出电压测量为0。

栅极电荷量(Qg) 198nC@10V
输入电容(Ciss) 13.5nF@50V

是不是LM5069栅极驱动电流太小,内部有一个保护机制? 对mos管Qg或Ciss是否有要求?