This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: 关于TIDA-010216设计中的一些问题咨询

Part Number: BQ76952

TIDA-010216: MOSFET Q32 control - Simulation, hardware & system design tools forum - Simulation, hardware & system design tools - TI E2E support forums

上述帖子中的以下内容该如何理解:

问题1:PDSG场效应管关断后(通过PACK_ADC可检测预放电完成状态),PACK_EN场效应管即转为关断,非常明确PACK_EN场效应管后关断;但是前半部分:在PDSG场效应管导通时,PACK_EN场效应管将首先保持导通状态,这句该如何理解,到底谁先导通?

问题2:上述既然非常明确PDSG场效应管先关断,PACK_EN场效应管后关断,我的疑问是:PDSG场效应管关断后,也就是预充完成,就切换到主MOS导通,那如果PACK_EN场效应管还没有关断会有什么问题?因为下文中第一条要求:当两个 CHG/DSG FET 都关断且未连接负载/充电器时,FET (PACK_EN)将导通。

问题3:原理图中的Q19 FET和Q33三极管部分电路的作用是什么,什么工作原理?

Here are the cases for the PACK_EN pin.

  • When both CHG/DSG FETs are OFF and if there is no load/charger attached the FET (PACK_EN) will be ON.
  • If a charger is attached, the FET (PACK_EN) will turn OFF to disable the circuits.
  • If a load is attached, the FET (PACK_EN) will initially be ON as the PDSG is turned on, then it will turn OFF after the PDSG FET turns-off (End of pre-discharge is known through PACK_ADC).
  • If a reverse charger is attached, the FET (PACK_EN) will be ON.

The MCU would keep PACK_EN low (OFF) in all other conditions.