Other Parts Discussed in Thread: LM3414
用于驱动3w的led灯,可以通过外部输入的电压控制信号来控制芯片电流的输出与截止,能够满足10kHz的LED开关频率,输出电流的波动小于5%。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM3414
用于驱动3w的led灯,可以通过外部输入的电压控制信号来控制芯片电流的输出与截止,能够满足10kHz的LED开关频率,输出电流的波动小于5%。
能够满足这样的需求的IC太多了,你可以把你的要求列的更为详细点,此外推荐你去TI官网webench的在线选型仿真软件去选择合适的方案。
多谢,webench确实很棒。具体的要求是:电压控制信号的范围为0~3.3v,芯片的供电电压15v左右,用于驱动一颗3w的cree的LED灯,最主要的是能满足10kHz的开关频率,芯片的惯性延迟要尽可能的小。
嗯,多问一下,为什么一定要10kHz的开关频率? 输出驱动LED电流需求多少?需不需要调光?
因为要做多通道的小型化PCR的光学模块,要保证至少在0.5ms内完成6个通道采样即完成6次的led的开关,同时进行采样,系统响应的速率越快越好。需要调光,准备用滤波后的PWM做压控信号,输入信号高于3.3v也可以接受。电流驱动为350mA~1000mA。谢谢啦。