This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100 容量缩放问题

Other Parts Discussed in Thread: BQ34Z100

            疑惑 :  手册上写容量缩放可以用Design Energy Scale这个参数来设置,个人认为这个值只用用来缩放Design Energy,Design Capacity和Design Energy两个参数都超过32767的时候对这两个参数缩放可以使用不同的比例,不知道是不是这样的?

举例   使用单节电池3.2V 1.5A的磷酸铁锂电池27并后两串,采用缩放和不采用缩放参数配置如下

                                                    不缩放                              缩放

        Design Capacity             40000                             20000               系数为2

         Design Energy               256000                          25600                系数为10        Design Energy Scale参数设为10  同时SCALED flag 置1

       Taper Current                  100                                     50

      Min Taper Capacity           25                                   12.5

        CC Threshold                 36000                             18000

  Dsg Current Threshold         60                                    30
Chg Current Threshold           75                                     38
Quit Current                               40                                     20

       Qmax Cell 0                  40000                                20000

    放电校准电流                     实际值                            实际值/2

其他的参数只要是电流的就改为1半,其他的一样,请问这样操作对不对?