如题,TPS23753 detection不成功,但是强制供48V是可以正常工作的,插上标准PSE供电设备,48V输出端每隔20ms会输出一个1.4V的电平,电压却不能持续上升,我是按照参考设计做的隔离电源,尝试了再输出端低压5V侧加15ma假负载,但是现象和之前一样, 另外也尝试了在48V测加了假负载,然后再测量48V输出端就只有0.2V左右了?请TI的大神指点下!!!谢谢!我把测试波形图给附上
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,TPS23753 detection不成功,但是强制供48V是可以正常工作的,插上标准PSE供电设备,48V输出端每隔20ms会输出一个1.4V的电平,电压却不能持续上升,我是按照参考设计做的隔离电源,尝试了再输出端低压5V侧加15ma假负载,但是现象和之前一样, 另外也尝试了在48V测加了假负载,然后再测量48V输出端就只有0.2V左右了?请TI的大神指点下!!!谢谢!我把测试波形图给附上
请看一下:
1. R47电阻实际阻值是否正常,焊接是否有问题?
2. PSE换一个其它的PD设备是否能上电?
3. 该PSE输出直接接一个24.5kohm的电阻,这个波形是什么样的?
Hi
从您描述来看,应该是detection出了问题。
detection过程除了电阻范围有限制,对电容也有150nF的限制。您可以把C59去掉看下。谢谢。
您好 将C59去掉 没有任何改变,另外我的RJ45是这样的(附件),应该是不支持通信线对供电的?
Hi
强制上电是会工作的,因为TPS23753工作的机理是如果VDD电压超过35V则会开始上电。你原理图中的两个整流桥都有焊接吧?谢谢。
The PSE drives the PI voltage to the operating range once it has decided to power up the PD. When VDD rises above the UVLO turn-on threshold (VUVLO-R, ~35 V) with RTN high, the TPS23753 enables the hotswap MOSFET with a ~140 mA (inrush) current limit.