This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9248PFC与PTD08D210W调试无电源输出

Other Parts Discussed in Thread: PTD08D210W, UCD9248, UCD7242

按照ZC702开发板搬过来的电源方案,将开发板配置程序导入到自己设计的板子后,电源无输出,求指点。

  • 亲;建议传个原理图并表明各点实测电压。象这样不工作的原因太多了,象管脚虚焊;过欠压外设不合理等等都有可能无脉冲输出。

  • 断电的时候测了一下PTD08D210W的输出,发现五片芯片的十路输出里有四路输出和地短在了一起,而这四路恰好是之前无论如何输出电压都是0的,这种情况是误操作导致芯片烧毁了吗?还是这种芯片带自我保护输出不正常时自动将输出短路了

  • 您好,我想问一下PTD08D210W使用方面的问题,UCD9248配置PTD08D210W,在线配置完后发现PTD08D210W输出电压为零,并且温度在5s内上升到了80度,断电后发现PTD08D210W的输出是和地短路的,但是配置之前PTD08D210W的输出并没有短路到地,并且再次上电把Flash擦除后掉电测量输出依然短路,尝试着把电源模块上的输出电容拆下后测量,发现电源模块上的UCD7242的电压输出引脚是和芯片的地近似短路的,电阻只有几欧姆。这种情况是因为PTD08D210W芯片损坏吗?