Other Parts Discussed in Thread: TPS5430, LM2576, TPS54260
各位工程师,你好。我现在一个项目需要用TPS5430,我的要求是输入18~28V,输出-11V~-10V,电流至少0.5A。请问怎么用TPS5430实现输出-11V~-10V,有什么要注意的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
做了一个实验:利用TPS5430将24V转成-12V,然后负载接一个滑动变阻器,当滑动变阻器小于11欧姆时,电路不能正常工作,测得负载上电流差不多为1.2A。这个耐压说的是??
Hi
-12V实际上是芯片的GND电压shift得到的,也就是最低电压,而最高电压是24V, 那么实际芯片的Vin和其GND的压差就是24-(-12)=36V,而datasheet推荐输入电压的范围最高是36V, 这就比较margin了。 如果输入时28V就是40V, 这个已经超过,就存在风险。
Hi
对于这类反向输出的设计,输入电压减去输出电压不得高于芯片推荐的最大供电电压。