This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2808-1: 是否可用于半桥拓扑应用

Part Number: UCC2808-1
Other Parts Discussed in Thread: UC3825,

您好,我设计一款半桥拓扑的电源,希望能够像反激电源芯片那样通过高压对启动电容充电,启动后由变压器辅助绕组供电(不想再做一个辅助电源给芯片供电),同时具备逐周期限流功能。我看了UCC2808-1和UC3825这两款芯片,典型应用是推挽拓扑,但官网中显示支持半桥拓扑。我计划芯片PWM输出驱动变压器,变压器副边两个绕组分别驱动上管和下管。不知道是否可行?如果不行是否有推荐的电源管理芯片或解决方案,谢谢!

电源主要技术参数:

输入电压:DC500V~1000V

输出电压:24V

输出电流:25A

输出功率:550W

最大效率:≥92%

开关频率:50kHz