1、芯片内部boost升压电路的开关频率是什么范围,负载接射频电路会有干扰吗?
2、芯片的使能引脚EN,高电平要大于 VBAT_SEC - 200mV,也就是说必须要用VBAT_SEC电源供电的运放来驱动吗,如果是请推荐一款低功耗和低价格的轨到轨运放。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
1. BQ25505是采用PFM形式的升压,最高频率达1MHZ,射频电路如果对噪声敏感需要考虑加LDO滤波;
2. 可以考虑用运放来驱动,看看TLV316合不合适。
谢谢你完美的回答,另外这款芯片的冷启动是怎么实现的?
比如我想要2V的电压输出,但是一开始储能电容上面的电压只有1点几伏,这时候芯片使能后升压电路会给电容充电,不可能在短时间内输出2V?
Hi Xuetao
BQ25505的最大持续充电电流为100mA,这个还是取决于你的电容是多大的,另外还有你能提供多大的一个输入。
但是理想情况下,总是需要一定时间的吧,需要在特定情况下来评估。