This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:学习状态停在了05,怎么办?

如图,使用的2A的锂电池,在学习的过程中先充满静置到05,Qmax Cell 0更新为实际值,由2000更新成了2108,VOK清零,然后以396MA的电流放电,放到电压为3V的时候去掉负载静置,可是放了一晚上了状态寄存器还是05,电压降到3v的时候断开负载,到今天早上变成3.517V了,化学ID为3531用你们的例程软件算出来的,这个是哪个地方不对呢,是不是没放完可以接着放电吗?

20160405.xls
  • 你的log数据很乱,放电过程不连续,放电过程中RUP_DIS bit置起来,即禁止Ra更新。所以Update Status不能更新到06。建议重新做golden learning。

    golden learning流程是电芯放空,静置5小时,发送0x0021命令,然后开始以0.5C充电,到FC bit置位后,静置2小时,开始以0.2C放电到放空,然后静置5小时。建议全程log数据。