Part Number: UCC25800-Q1
我们的设计条件为输入9-15V,标称输入电压为12V,需求输出为24V,输出功率20W。
倾向的电源管理芯片的拓扑为谐振LLC电路,因此选型了UCC25800。但是通过查阅Datasheet和仿真后发现这款芯片满足不了我们现在的设计条件。
请问有没有同样为谐振LLC拓扑的电源管理芯片可替代UCC25800?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: UCC25800-Q1
我们的设计条件为输入9-15V,标称输入电压为12V,需求输出为24V,输出功率20W。
倾向的电源管理芯片的拓扑为谐振LLC电路,因此选型了UCC25800。但是通过查阅Datasheet和仿真后发现这款芯片满足不了我们现在的设计条件。
请问有没有同样为谐振LLC拓扑的电源管理芯片可替代UCC25800?
在20W时,我们没有任何集成FET的LLC控制器。另外,我觉得输入从9-15V变化,需要来自输出的反馈来保持恒定的输出电压(24V)。在这种情况下,可以根据电压和电流要求使用LLC控制器UCC25600和2个外部FET,也可以添加光耦合器以获得原边侧的输出反馈。
此外,如果从LLC转移到原边调节反激式架构(Primary side regulated Flyback)可以节省一些成本,例如LM25185。
通过下面视频以及同一研讨会的PPT可以了解这些拓扑结构的优缺点:
Isolated gate-driver bias-supply design considerations | Video | TI.com