bq27411芯片IIC通信,芯片怎样初始化配置,不初始化能不能读取电压参数,我现在没做什么配置直接读取电压寄存器,读出来的事0,求解答下,大神!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个芯片是需要OTP烧写的,不过应该是上电就可以读出电压的,请确认一下读取的寄存器是否正确,另外如果不是放在电池包里的话建议使用BQ27441,这个参数在RAM里配置,也比较简单。
你好!
我正在使用27411,在考虑是否要更换27441,我有三个问题。
Q1:请问27411的OTP烧写,烧写的是哪些参数?
我读了27411的datasheet和它的Techenical Reference,还是没有找到OTP烧写的参数。
《SmartFlash OTP Programming(SLUA703)》我也没在TI网站上找打。
Q2:27411如果不使用OTP编程,是否可以直接通过访问它的Data Memory来写入相关参数?
我看Techenical Reference是这么说的:
另外,在Techenical Reference的3.1节,还给出了一个修改Design Capacity的例子。
是否表示不用OTP,也可以通过软件来配置这些参数?
Q3:我看了27441的datasheet:
27441也要用OTP烧写?
谢谢!
Frank