This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问48V输出有带负载测试么?请附加未加三极管和加了三极管的驱动波形对比。
请把三极管电路贴出来方便分析。
增加电容后,是这样理解,但是增加之后的电容也最大到1500uF,对12V电源来说这个应该不算很大吧?
我用的是直流稳压电源输出,规格是12V-5A的,我们的产品正常跑是3A电流稳压电源都能正常工作,
对于这个瞬间电流也太恐怖了吧?
还有增加三极管之后我把LM3478拆下来是板子的其他电路是可以正常运行的,三极管有2V的压降,但到输入
引脚的电压也有9V-10V,焊上LM3478之后就会出现上电瞬间电流过大的现象!!
各位大神,求救呀!!!
Hi Yun
谢谢把原理图贴出来,这样方便理解多了.
1. 首先你用TIP112大概是用作输入缓起作用,但是我看了下这颗物料的电流大概就2-4A,是不合适的,建议你还是使用MOSFET或者用我们TPS2592BL作为你12V输入缓起和电流保护;
2. 输入1000uF电容相当于是你的适配器的输出加电容,启动保护不是说你的适配器可以支持4A电流就可以说完全没问题,可能有两方面原因,一个可能是你的适配器后端加大电容可能导致不稳定,也有可能输出就是不能支持这么大电容启动,可能保护了。
整个系统起来之后再启动3478吗?有3478的这块板,正常运行的时候就只有150mA的电流,整机稳定时的电流就有1.6A,
现在加了三极管之后,使用的直流稳压电源与适配器(12V/5A)都一直是这个现象!
把3478输出电容调小了,还是会出现保护!!
还有什么好的办法不?大神?
升压芯片在上电瞬间给输出电容充电,会有一个比较大的瞬间电流,延时上电,就是先用Vin让输出电容充满电,然后再使能(Enable)控制器,上电时就不会看到瞬间大电流