1、我根据battery management studio中新建工程,依次配置好了Design Voltage和bq27441的QuickStart Guide中提到的那4个基本参数(Design Capacity、Design Energy、Terminate Voltage和Taper rate)。(PS:设计电压3.7v,设计容量6400mah、设计能量23680mwh、截止电压3.4v、TaperRate值178),再进行了校准,然后执行Learning Cycle。过程是按照www.deyisupport.com/.../46539.aspx官方论坛中的帖子步骤来的,先准备3.0-3.3v的空电池,静置,然后连接评估板,进行了如上的配置和校准,在充完电静置过程中,“ERR:[QMAX_UP:Not Set]”错误。如图:
2、在www.deyisupport.com/.../46539.aspx“循环学习和导出量产文件”的步骤D中,为什么要确保Update Status的值为0x06?在Technical Reference(Page 42)中,说的是Update Status的bit0和bit1作用是决定能够更改Qmax和Ra Table值。只有当learning cycle将要完成时,bit0和bit1才要被置位————这样子的话,学习结束后也应该确保Update Status值为0x03啊,怎么会是0x06?
对了,我使用的工具是bq27441评估板,EV2300,配套软件是bqStudio1.3.45。希望有熟悉电量计使用的朋友能帮一下忙,先在这谢谢了!