请教TI的工程师,我想给一组3个并联的18650锂电池充电,单个锂电池容量为2400mah,充电电压为4.2v。板上供电电压为5v,请问我该选择ti的哪款管理芯片?随便请教我需将4.2v电压升至5v输出,输出最大电流为3a,同求升压控制芯片
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
关断模式就是芯片不工作,输出为0V。comp是环路补偿功能,补偿芯片里面运放的稳定性。可以用webench直接仿真设计comp参数
http://www.deyisupport.com/question_answer/analog/battery_management/f/35/t/104855.aspx
如果充电需要达到3A,那么使用USB接口充是达不到要求的,需要使用高压适配器。高压适配器可以使用固定输出的和自动升压的。固定输出的适配器可以使用BQ24195实现充电,自动升压的可以使用BQ25895实现。如果充电和升5V输出不需要同时工作,那么可以使用充电芯片的OTG实现,如果需要同时工作,可以使用TPS61253或者61088一类的实现。