This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于两节3.7V锂电池共同工作并充电的问题

目前设计的产品中由于空间所限,需要放置两块容量不一的3.7V锂电池,一个容量为500毫安时,一个230毫安时左右。现在需要两块电池共同工作,不知道电池应该串联还是并联。还需要支持USB为电池充电,我怕因为容量不一放电充电过程中因电池容量不一出现问题,求一个解决方案,谢谢!

PS:板子主芯片可接受3.6V以下的电压,但是GPRS模块电压低于3.3V会停止工作。

  • 最好是两个相同的电池并联或串联充电,这样电池的电气特性可以基本一致,如果你这种情况最好还是并联充电,需要注意充电电流不能太大,差不多也能满足你的系统需求。