This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS43060: tps43060 PIIN VIN and PIN VCC short

Part Number: TPS43060

I designed a boost boost circuit using the TPS43060RTER, with an input voltage of 5V, an output voltage of 32V, and a switching frequency of 270KHz. Connect the output to a light load, and the output current is approximately 5mA. After the circuit has run several times, it will start abnormally. After measurement, it was found that the VCC and VIN pins of the chip were short-circuited.SCH_POWER_3_3-BOOST_2025-12-24.png