This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54331: TPS54331技术咨询

Part Number: TPS54331

你好,

     想咨询关于TPS54331芯片的应用问题:输入8-10V,输出通过反馈电阻设置为5V,带载1A,电感使用贴片电感-CD54-220-22uH±10%-NiZn F4R CD54-1A-CLASS B-5.8*5.4*4.5mm,没有搭建电路实测,不知道是否有风险,请给些建议,谢谢!

 

  • 您好,

    这个电感的饱和电流是1A?若是,对于设计输出1A的话有点小(芯片数据手册8.2.2.5.1 Inductor Selection)。

    您可以使用WEBENCH设计工具辅助设计,并参考其BOM。