工程师你们好,目前我们正在使用BQ25750开发一款UPS产品,在调试过程中发现mos温度有点异常,采用的30V10A充电器,设置的充电电压为29.4V,7串三元锂电池,充电电流8A,电池从21V开始充电,电流8A最高温度68℃,一小时后温度维持在60℃左右趋于稳定,但在电池冲到25.89V时出现温度异常,温度在十分钟内急剧升高15℃,由61℃升到76℃,之后最高温度达到115℃。我们分析跟电压有关系,一开始8A充电一小时,温度趋于稳定,大于25.89V,温度无法稳定下来。于是我们做了第二次测试,让电池从26.35开始充电,温度没有出现稳定现象,从室温29℃一直升到120℃。可以帮忙分析下是哪里出现问题了吗?