Other Parts Discussed in Thread: TPS54240, TPS54327, TPS62130A
TPS54240设置输出电压为4.2V, 为何输入电压为5V不能工作,有些芯片要到6V才能稳定工作?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是不是5V输入的时候,在轻载或者空载情况下工作,4.2V不稳定?加500mA负载,如果能正常工作的话,请参考下面这个文章。
http://www.ti.com.cn/cn/lit/an/slva547a/slva547a.pdf
如果是低压输入电路,没必要用tps54240,用tps54327就可以了。
Hi
受限于最大duty, 但是84%的看空比应该问题不大。
注意将输入电容加大一点,尽量靠近芯片Vin脚。
Hi
或者选用一些高duty的芯片,例如TPS62130A: http://www.ti.com/product/TPS62130A