BQ25895在外部充电器介入后会首先判断对方是不是快充充电器。然后由单片机控制BQ25895让快充输出一个制定的电压。
请问,我在我的设计中使用了一个BQ25895,我不使用D+,D-来判断外部充电器是否可以快充,也不用单片机来控制外部快充的
输出电压。我直接用一个12V或者9V电源接到BQ25895的VBUS上,请问这可以实现快充吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ25895在外部充电器介入后会首先判断对方是不是快充充电器。然后由单片机控制BQ25895让快充输出一个制定的电压。
请问,我在我的设计中使用了一个BQ25895,我不使用D+,D-来判断外部充电器是否可以快充,也不用单片机来控制外部快充的
输出电压。我直接用一个12V或者9V电源接到BQ25895的VBUS上,请问这可以实现快充吗?
没有问题的,BQ25895支持12V输入,这么做的主要目的只是为了使USB适配器默认输出为5V防止烧坏不支持高压输入的charger才有握手协议这个说法,如果适配器不插别的,直接给高压是最方便的
谢谢您的回复!
如果我直接用快充适配器连接到BQ25895器件上,不考虑握手协议的事,是不是可以不用考虑用单片机来读写BQ25895的IIC寄存器了?
谢谢!
需要看一下charger的默认充电电流,充电电压,输入限流是否合适,一般情况下这些值都需要重新通过单片机进行设置。谢谢!
硬件电路设计好了,不需要I2C参与也是可以实现升压充电的。如果不充电,是不是TS脚的电压不对?