需求:
输入电压—— 12~60VDC
输出 —— 8V/10A
低纹波。
看了一下资料,LM5085 和 LM5088 标称能做到15A,
从价格上5085是首选,但是,需要做到10A 电流,
都能实现上述需求吗?设计中有哪些需要注意的地方,才能完美输出?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好 Chun Li
两个芯片都不推荐做你的应用,因为你需要的电流比较高,所以需要把效率提高来减小你的热损耗。LM5085是PFET驱动,效率不够,LM5088是非同步方案,一样的问题。
我推荐给你LM5116. http://www.ti.com.cn/product/cn/lm5116/description,高压同步控制器,在链接网站你可以看到相应的Webench设计帮你设计参数和原理图。