用tps563200输入9v,输出4.1v.现在测下来波形是这样的。
原理图如下:
纹波能不能控制在20mv内?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输入输出电容电感怎么配置才能使纹波峰峰值缩小在20mV内呢?
另外带载1A后会出现电压不稳的情况,4.3v最低的时候只有3.2v左右,等稳定后也会降0.3v的电压。有什么措施能稳定电压,波动在0.3v都内都可以接受。
希望给予技术上的指导,谢谢!
Hi
电路,您可以用TI的webench仿真软件得到: http://www.ti.com.cn/product/cn/tps563200
或者参考datasheet : http://www.ti.com.cn/cn/lit/ds/symlink/tps563200.pdf 第十四页等也行。
重点要注意输出电容的ESR(,见datasheet,选择的是the typical ESR is 2 mΩ each.)和layout.