This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610充放电电路问题咨询

Other Parts Discussed in Thread: BQ24160, BQ24610

  目前我们BQ24160充放电电路输入端防反插用的是TI针对BQ24610推荐电路,由于SI7616芯片原厂已经停产,规格书也未找到,对此MOS的性能不太了解,本想用SI7617 P-mos替代SI7616但是发现不行(PG脚对应的指示灯闪),感觉是欠压了,请问SI7616为何在此处不能用SI7617替代,具体此MOS性能及此在此电路中如何工作还请告知一下,又或者你们帮推荐下相关与si7616的替代型号,此方案是用于DLP投影上,充放电目前倒没有发现什么问题,工作正常,以上请帮解答下。


  • 请问为什么19V供电就PG脚对应的指示灯就不会闪,工作也正常,求大神指点下,感谢

  • 用TI的BQ24610推荐电路,目前我想用推荐电路中SI7617替代SI7616 P-MOS管,目前我电池为3节,电池电压为12.6V,当我用12V外置adapt供电会出现电压输出不正常现象(第8脚指示灯会闪烁,不正常),电压也不稳定,而用19V外置adapt供电就不会出现输出电源不正常问题(第8脚灯不会闪烁,正常),电压此时比较稳定,我分析是否因为用12V输入时ACN脚对应的电压要比SNR脚对应的电压小于200mv导致,处于临界状态导致,固第8脚才会灯闪。但那又为什么我用SI7616用12V外置adapt就不会出现输出电源不正常现象,这又有点矛盾了,就大神帮指点下,真的是比较着急,感谢指导。

  • 你好

      BQ24610是降压充电芯片,当你的输入为12V,是不可能给你的12.6V电池充满的。

  • 问题还是电压低于电池的设定电压,谢谢的回复,已经知道原因