This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5117,上MOS开通瞬间,下管驱动波形出现振荡;电流超过3A时,开关频率降为设定值的一半,MOS驱动波形出现大量的窄脉冲

如图,硬件原理图基本同TI的官方DEMO板,电感更换为15uH,MOS管更换为仙童的FDP150N10,不使用内部LDO,VCC由外部13.4V电源供电。

主要出现问题有两个

1)上MOS开通瞬间,下管驱动波形出现振荡,振荡幅度可达±10V以上,频率在55M级别;

2)电流超过3A后,开关频率降低为120KHz(原来为230KHz),MOS驱动波形上出现窄脉冲(窄脉冲的出现频率大致为230KHz,约等于设定的开关频率值)。

     若通过加大RT来增加开关频率如调整为470KHz,实测频率仍然不变为120KHz,,而窄脉冲频率变化为470KHz。