This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电池管理芯片咨询

用TI的BQ24610推荐电路,目前我想用推荐电路中SI7617替代SI7616 P-MOS管,目前我电池为3节,电池电压为12.6V,当我用12V外置adapt供电会出现电压输出不正常现象(第8脚指示灯会闪烁,不正常),电压也不稳定,而用19V外置adapt供电就不会出现输出电源不正常问题(第8脚灯不会闪烁,正常),电压此时比较稳定,我分析是否因为用12V输入时ACN脚对应的电压要比SNR脚对应的电压小于200mv导致,处于临界状态导致,固第8脚才会灯闪。但那又为什么我用SI7616用12V外置adapt就不会出现输出电源不正常现象,这又有点矛盾了,就大神帮指点下,真的是比较着急,感谢指导。

  • 电池在放空的时候充电应该是正常的,这时是在fast charging current regulation phase,

    到后面不正常是因为电池进入fast charging voltage regulation phase,

    这时外部charger只有12V,电池充饱电压要12.6,当电池电压到12V就没办法再充电了,换成19V就能继续充。

  • 这是buck拓扑结构的充电器,即使采用P-MOSFET不需要refresh 自举电路实现近100%占空比,考虑到一些效率因子损耗和buck本身的拓扑结构,还是要保证输入电压略大于CV电压以保证能够进入稳态。