This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65130的输出不正常,空载可以,加AD5762R之后不正常。



1、5V输入,芯片上电之后(带负载AD5762R),负端输出约为0.3V左右,正端输出约5V左右;这时,si2323DS(Pmos)的G端电压为0.5V左右,S、D端都为5V,芯片的FBN电压都不正常约1.2V(应为0V)。

此时,如果将G端接5V,2秒后断开,G端电压变为0V,负端变的正常,为-13.2V左右,正端也正常了13.2V左右,电压很稳定。

2、用电阻替负载AD5762R,发现当电阻为3K左右时,负电压开始拉低。

3、空载时正常,正负13.2伏左右,但是电压不是很稳定,芯片有噪声,滋滋的声音,声音有点大。这个芯片以前用过,比较以前的,噪声没这么大。

各位高手帮忙分析下原因,谢谢!原理图如下。

biaozj.pdf