Part Number: LM74810EVM
您好,关于LM74810 在48V车载系统中,TVS的选型,请麻烦给出建议
- 运用在48V新能源车载系统,电池正常使用范围为40V到60V
- datasheet中推荐了12V系统和24V系统的TVS选型建议,请帮忙给出48V系统的TVS选型建议
- 请帮忙给出48V系统的MOSFET选型建议
感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM74810EVM
您好,关于LM74810 在48V车载系统中,TVS的选型,请麻烦给出建议
感谢
您好,
请参考此贴中的回复,如果对回复有疑问您可以直接跟帖继续提问,e2echina.ti.com/.../lm74810evm-lm74810-48v-tvs-mosfet