设计电路时发现一个问题,BQ51050只有一个状态输出引脚CHG,如何区分:不在充电、正在充电、已充满电这三个状态呢?如果说这个问题可以用测量电池电压来解决的话,那还有另一个问题,我的电路在关机的时候LDO后边全部断电的,如果这时进行无线充电,必须由BQ51050提供一个使用信号让LDO工作。请问有没有比较好的解决方案?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
设计电路时发现一个问题,BQ51050只有一个状态输出引脚CHG,如何区分:不在充电、正在充电、已充满电这三个状态呢?如果说这个问题可以用测量电池电压来解决的话,那还有另一个问题,我的电路在关机的时候LDO后边全部断电的,如果这时进行无线充电,必须由BQ51050提供一个使用信号让LDO工作。请问有没有比较好的解决方案?
Hi Xiaolin
你可以直接使用CHG信号来用来使能LDO的工作
谢谢!
谢谢,不过CHG是开漏极输出(open-drain),充电时此管会打开,上拉的话也是低电平输出,而LDO使能端是高电平有效,直接使能不行吧?如果加反相器的话,第一,此时LDO没有输出,如果使用电池直接给反相器供电,会使电路无法关机。