Part Number: BQ25750
Other Parts Discussed in Thread: BQ24610
Can the BQ25750 switch the power path by itself like the BQ24610, without relying on software control?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thank you for your reply. I have one more question: when the BQ25750 is configured in reverse mode (i.e., automatic power path switching) with the adapter supplying power for the first time, and then both the adapter and battery power supplies are disconnected. Can the system still be powered normally by the battery when only the battery is connected afterward?
您好,
reverse mode 是应用于在没有输入源的时候,通过电池给系统供电。
如果输入源和电池都移除,那么芯片下电。再插上电池后,芯片启动,执行“8.3.2 Device Power-Up From Battery Without Input Source”。