This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB给锂电池充电,稳压在3.3V,温度变化会影响3.3V的输出



综述:我做一个USB给锂电池充电,稳在3.3V,(要求3.3V,0.5A)。原理图见附件。

测试现象描述:

1、发现一个很奇怪的现象,温度变化会影响LDO的3.3V的输出。有时有稳定的3.3V输出,有时根本没有输出,0V。

2、温度变化指的是在开空调的房间(23℃,实际温度计测试25℃)和在室外或者没有开空调的房间闷热(温度计测28℃~29℃)。

3、开空调的房间,测试LDO的输出电压,是断断续续的,时而有3.3V输出时而输出电压0V,时而电压不稳3.1V~3.2V。

4、室外和不开空调,测试很多次都是稳稳的定在3.3V的输出电压上。

5、电池是锂聚合物电池,容量500mah左右。

6、LDO用的是TI的TPS73733,在淘宝购买,不能确认是正品。

7、充电电路的前半部分是南京拓微集成电路的TP4056,电路也是按官方提供连接,去掉了temp脚的连接,直接到GND,电池温度检测取消,不影响其他功能。

分析原因:1、可能管脚虚汗,用电烙铁又焊了,此项暂时排除。

         2、LDO工作环境,和温度关系大,查资料datasheet说-40℃~125℃应该都可以工作。

  • jobs ding,

         附件中没有原理图,请上传,谢谢。“使用高级文本编辑”中的“添加附件”。

  • -40℃~125℃是芯片的使用环境温度,但是同时还需要满足芯片的结温要求,芯片结温超过160℃,芯片shutdown,

    Tj= Ta +Rq* Pd      Ta是环境温度,Tj最大160℃,推荐为125℃, Pd=(Vin-Vout)*Iout是芯片功耗,Rq是热阻, 所以实际上芯片能使用的环境温度不会是-40℃~125℃。

    能否说明你下您输入输出负载条件,确认是否因为芯片过热导致的,或者可以用手指测一下,有条件就测试一下芯片结温。  您能选用TPS73733代表负载很大,要尽量降低输入输出电压压差,同时要注意散热设计。